Hi,
Could anyone tell me the difference between Switching Valley current and Dc current.
what will be the maximum output current for TPS61253A
1. 1500mA or 4A ??
If i had a load of 4A, will it discharge the battery at 4A? (Battery used 5200mah)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could anyone tell me the difference between Switching Valley current and Dc current.
what will be the maximum output current for TPS61253A
1. 1500mA or 4A ??
If i had a load of 4A, will it discharge the battery at 4A? (Battery used 5200mah)
Hi Sir,
The DC current means the output current during the pre-charge phase, during the pre-charge phase, there's no switching.
The switching valley current means the inductor valley current after the pre-charge phase, Vo>Vin-0.3V at this phase.
The maximum output current capability of TPS61253A is 1.5A@Vin=3V , 1.75A@Vin=3.6V, 2A@Vin=4.2V. it can't support 4A output load.
Could you please share the detailed application information with us? my email address is helen-chen@ti.com