This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help charger BQ2057T.

Other Parts Discussed in Thread: BQ2057T

Help charger BQ2057T.
Used BQ2057T, from http://www.ti.com/lit/gpn/bq2057t
Figure 4. 0.5-A Charger Using P-Channel MOSFET with the following changes

MOSFET - IRF7424
Rsns = 0.33 OHM

When power up (Vin = 8.90V is obtained pulse signal on output pin CC
See link below:
http://www.mypicx.com/08102010/P1/

This occurs in rare case, and is different from the linear control signal. Charge current is about 200mA (shortly after leaving current limit of 350mA in my case)
This is normal behavior BQ2057T?

10X