Part Number: TPS92515HV
Other Parts Discussed in Thread: TPS92515
Hello,
I'm developing 2 different boards with TPS92515HV.
First board has 12V 6W LED, 48V as Input voltage
Second board has 30V 26W LED, 48V as Input voltage
Sometimes happens that TPS92515HV blows-up (it's phisically broken) when board is connected to powered-on lab power supply (hot plug) with 30inch cables,.
It happens also using evaluation TPS92515HVEVM at 48V (replacing TPS92515 with HV one).
I read this:
https://e2e.ti.com/blogs_/b/fullycharged/archive/2015/05/20/what-is-that-giant-tantalum-cap-on-the-input-of-the-evm
I'm worry about this problem because boards have some precautions:
* 56V fast transient voltage suppressor on input line (SM15T56AY)
* Limited input inrush current using MOS on GND line (MOS is driven by RC network). It give Vin similar to Figure 36 of datasheet.
but it happens anyway: sometimes TPS92515HV (and few times also MOS transistor) blows-up when I connect the board to 48V.
Do you think that it should be caused by voltage spike of power supply?
Do you have some suggestion to give me to make boards more strong?
Thank you a lot!