This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3801: /RESET pin status when TPS3801 is lower than 1.1V

Part Number: TPS3801

In TPS3801 datasheet, Timing Diagram is shown as below.

When VDD is lower than 1.1V, the /RESET pin status is seems uncontrolled? Right?

Do we need to add a resistor with GND to keep /RESET low?

Thanks.