Other Parts Discussed in Thread: TPS61230
I am using the TPS61200 (adjustable) reference application circuit on page 14, where I am connecting a single-cell lithium polymer battery (3.7V nominal) as the input supply, and I am setting the regulator (R1, R2) to 4.7V output. The circuit works fine, but when trying to configure it to use UVLO as a battery saver, it seems unable to be set in a way that makes sense for a 3.7V lithium polymer input source. I want to set the UVLO threshold for 3V input, which is the recommended lowest battery voltage to allow it to drain down to. So I have a 249K resistor (R4) to GND from UVLO, and a 2.7M resistor (R3) from Vin to UVLO. This results in 0.25V at UVLO when the input drops to 3V. It seems the regulator won't even turn on when I do this, and it may be because at 3.7V input, the voltage at UVLO may not be above the minimum required based on the chip tolerances I see in the datasheet. I don't see how you can use UVLO reliably to do this for a 3.7V battery and have a reliable 3.0V cutoff, and also make sure it will work if the battery goes above say 3.2V. What am I missing, or doing wrong here?