This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3875: inconsistant duty cycle value in UC3876 pin C and D

Part Number: UC3875


1.The periphery circuits of UC3875 is shown in figure 1. 

2.From the datasheet of UC3875 , I know the duty cycle of pin C and D  is complementary. If input voltage of pin NI is constant in one cycle,the output duty cycle of c and d is consistent. 

However, If  there is ripple from input voltage of pin NI in one cycle, the output duty cycle of c and d is not consistent.(the ripple of pin NI is hard to suppress)  ,as figure 2 shows.

3.question:how to keep consistent for duty cycle of c and d?or Can you recommend a kind of new chip for me?