Part Number: BQ24735EVM-710
Other Parts Discussed in Thread: EV2400, BQ24735
Tool/software: Starterware
Hi,
I cannot install GUI. (both win7 and win10)
My procedures are as follows;
1) Install Visual basic 6 runtime ->OK
2) I extracted all files from sluc258a.zip and excute out setup.exe.
3) Error message (1)
Install setup.exe - Bad image
VB6STKIT.DLL can't execute or included error
4) Error message (2)
Cannot start main setup program! (CreateProcess() returned error code 0x000000C1H)
5) Error message (3)
Setup will now start application removel utility to remove temporary install files.
5) Error message (4)
Error attempting to run the application removal program to remove etmporary installation fiiles.
Please teach me what is problem.
Regards,
PAN-M