Part Number: BQ25601
Hi Charger Experts,
I have two questions:
1. What is the REGN voltage when Vin is 12V? Datasheet only specs 5V and 9V input.
2. Using 9V or 12V as Vin has a gotcha/showstopper: The default REG06, OVP[1:0] bits are set to 6.5V by default - meaning that the part is disabled (no powerpath, no i2c) if you have a dead/missing battery and a 9V, 12V wall wart. This is a big deal. Is there going to be a fix for this? If not, can you please at least update the datasheet so that this nuance is in bold?
Thanks!
Jason