Hi,
What's the status of the DIO after power up if there is no code running?
What's the reset value of IOCFGx?
there is "6000h" in the 11.11.3.5 IOCFG4 Register (Offset = 10h) [reset = 6000h]
but, in the table, only bellow bit reset value is 3h, others are 0h.
14-13 PULL_CTL R/W 3h Pull control
1h = DWN : Pull down
2h = UP : Pull up
3h = DIS : No pull
BR. Albin