This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041: with 1 input half bridge gate driver

Guru 29690 points
Part Number: LM5041
Other Parts Discussed in Thread: LM5102, , LM5105

Hi Team,

The typical application shows LM5102 (2 input half bridge gate driver) for gate driver.



I believe LM5105 (1 input half bridge gate driver) is also usable with LM5041 and LD output of LM5041 should be left open in this case.
Is my understanding correct?

Best Regards,
Yaita / Japan disty

  • Hi Yaita-san,

    Yes you can use the HD output as the input to the LM5105 and leave the LD pin open circuit or I suggest a small load of 1k to ground to provide some load to the internal drivers and to slow down the switching edges.

    Why does the customer not want to use the LM5102?

    Regards

    Peter
  • Hi Peter-san,

    Thank you always for your kind support.
    I understood.

    >Why does the customer not want to use the LM5102?
    According to web price, LM5105 is a little lower than LM5102 so I would like to decide which device I should suggest.

    Best Regards,
    Yaita