This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 825
Part Number: TL5001
I am working on a design that will use the TL5001. It is a DC-DC high Vout flyback converter(Isolated DC/DC).
Issue:
1.I use 100K resistance between RT & GND, System work oscillator frequency is 22K when on load is 3W, 100K at no-load. Why not always 100K.
2.I need control dead-time at 4.5us,Dead-time will be longer when input form 8V to 16V, Another situation is duty cycle goes to 0%, Now TL5001 not work or transformer saturation.
How can I solve this question?Please help ,Thanks!!!
In reply to EricLee1880267: