Socket:TLV62090
Application:Vin:5V、Vout: 3.3V;Test Point:T97,up overshoot 1.65V、down overshoot 0.81V,we need control it small than 0.5V.
below is schematic and waveform, pls help check and give advise.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear customer,
I think that what you call echo in the picture is the conduction of the low side FET's back diode during the dead time.
Dead time is the time between on-and-off phases of low and high side FETs. It is needed in order to avoid cross-conduction between the FETs, which can cause damage to the device due to high currents, or loss in efficiency when the energy (current*voltage*time) during the crossoconduction is not enough electrical-over-stress. Hence I wouldn't worry much about that "undershoot".
I would rather check what happens when the high side turns off and low side turns on! I have highlighted in green in the picture below a weird oscillation, which shows the SW node suddenly going up for a little while..this is a possible sign that the high side is being turned on again before the low side back diode starts conducting the inductor current. Indeed you can see that there is no "undershoot". That means that the current may pass directly from the high side to the low side, and as a consequence, you may have the crossconduction mentioned above.
This behaviour of double turn on of the high side is caused by both the amount drain-source capacitance and the slope of the SW node (dV/dt*C=i) which can cause a current that charges the high side gate-source cap through the drain-gate high side parasitic capacitance, eventually turning on the device.
To better understand this behavior I recommend the reading of "Modeling switching losses in MOSFETs half-bridges", G. Di Capua, N. Femia, IEEE SMACD 2012.
Back to us, the device is designed to avoid this behaviour and allow the backdiode to conduct during the dead time. Indeed I think the snubber capacitors, especially C225, which are not mentioned in our datasheet's application example, are the cause of this effect. I would chose different values and dimension them so that you can see backdiode "undershoot" in the green oval.
If you have any question, don't hesitate to ask.
Best regards,
Emmanuel Granatello
hi: Emmanuel
It's not easy to find here, en..I'm design that schematic of TLV62090 APP. First I want to thank Mr. Liu (FAE of Ti) push my questions to here!
I improvement probe as follow...
Then let R312/R316/C222/C225 -> NC, probe L25(SW) & C215(GND) with BW=20MHz, Overshoot Like this...(216.6mV)
Again R312/R316/C222/C225 -> NC, probe L25(SW) & C215(GND) with BW=500MHz, Overshoot Like this...(1.497V)
If BW=500MHz, Overshoot is more than 0.5V, Maybe Lead to excessive EMC, Should I warry it?
Dear Emmanuel,
Thanks for your great support.
Update our test result as below. We found there is 1.497V overshoot when we use 500MHz bandwidth, we afraid that this may influence EMC test.
Would you pls share some experience and advice.
Thanks.
1、 Optimized Probe
2、 Remove R312/R316/C222/C225,Probe connect to C215(GND) and L25(SW),Bandwidth=20MHz,Overshoot waveform(216mV)
3、 Remove R312/R316/C222/C225,Probe connect to C215(GND) and L25(SW),Bandwidth=500MHz,Overshoot waveform(1.497V)