Part Number: TPS65131
I am having an issue where the negative converter voltage VNEGis -20V instead of the -15V its supposed to. I placed a decade box in place of R5 (see schematic below) but cannot get the voltage to lower, on top of that the voltage at pin 16 (FBN) is approx 0.4V instead of the 0V its supposed to be on the datasheet. Any idea where i might be going wrong? The input voltage is 5V from a USB port.
Edit:
Here is voltage waveform I am seeing on the FBN pin: