Hi Support team,
Could you please support us with some questions to design we made with AM3358BZCZA100 and TPS65217C PMIC.
We are facing some issues related to PMIC we think:
- VLDO1 of PMIC TPS65217C pin 3 voltage from time-to-time jumpes from 1.8V to 2V. The voltage is an output of an LDO, so we assume there should be stable 1.8V. What could be a root cause of the voltage jumping?
- When power to PMIC is switched off and on again in a short period of time, the board cannot start from time to time. Usual current consumption of board is 0.3-0.4 A, but if the issue occurs, the current consumption is 0.1-0.2 A and board is not running. PMIC outputs incorrect voltages, as a result, the CPU cannot start. Any manipulations with the PMIC (as reset pin, enable pin) could not restart the PMIC to normal operation. What could be a root cause of PMIC improper startup
Please also find attached schematic diagram of our design.