The Vref parameter is described on page 5 of the TPS 62065-Q1 datasheet.
Typical values are listed here.
However, min and max values are not listed.
Could you provide information on the min and max values of Vref?
-Harukawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Vref parameter is described on page 5 of the TPS 62065-Q1 datasheet.
Typical values are listed here.
However, min and max values are not listed.
Could you provide information on the min and max values of Vref?
-Harukawa
Thank you for your reply.
I could not find "spec table".
I might not understand your answers correctly.
Please tell me where "spec table" points.
(What page of the TPS62065-Q1 datasheet should be referred to?)
-Harukawa
Thank you for your help.
I am referencing a TPS62065-Q1 datasheet that can be downloaded from the TI page.
"VFB(PWM)" is listed on the next line of the Vref spec.
Is the min (-1.5%) and max (1.5%) listed are min and max of Vref?
Vref(Typ):600mV
Vref(min):609mV
Vref(min):591mV
Is this understanding correct?
-Harukawa