I built a circuit based on "Increasing Available Load Power in an LM2587 Boost Regulator" app note (its link is http://www.ti.com/lit/an/snva552/snva552.pdf). The difference is my input is around 24VDC, the output I want is 28VDC.
The circuit is working fine when there is no load at all! The output is 28VDC, and when switching the circuit ON/OFF, the circuit is working fine.
But when putting a load drawing current 1A, the input voltage drops to 3.5V insteading of 24V DC.
If I switched ON the circuit without load, then connected the 1A load afterwards, the circuit is working fine and the output is drawing 1A.
But if I switch OFF the circuit and then switched it ON (with the load connected), then the circuit failed to regulate. Any thoughts please?
Thanks in advance.