Other Parts Discussed in Thread: CSD87330Q3D, , TPS51219
Hi,
I have new request as follows:
- 20V nominal input, max acceptable up to 24V
- Max output current= 15.5A
- Output voltage= 0.9V
- Transient 0.8A =>7.3A in 2us (6.5A inrush in 2us) with less than 20mV drop
I identified tps53219a + csd87330q3d as good fit.
Customer would TI to confirm feasibility. One major concern is about voltage drop of 20mV for load transient 6.5A in 2us.
=> can we provide schematic to meet customer spec above ?
=> do we have simulation results or measurements to prove we can achieve customer spec for transient load ?
regards,
Paul