This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Question on BQ27426 reference design

Prodigy 220 points

Replies: 5

Views: 594

Part Number: BQ27426

I was looking in the schematic and layout of this ref design: www.ti.com/.../TIDA-01012

Wireless IoT, Bluetooth® Low Energy, 4½ Digit, 100kHz True RMS Digital Multimeter.  I notice BT1, terminal 2,  the negative terminal (pack-) is not connected to GND node -- the gate of the P-Mosfet (D3).

In fact I don't see the BT1 node 2 anywhere in the layout. Should it not be there?

If I decide to use this part in my design, should I not connect the BT1 battery negative terminal (pack-) to GND and P-Mosfet together? Please advise.

Also, I'll be using 3.3V for I2C interface, should I use 4.7K for I2C pull-up? I already use I2C in my board and has the necessary pull-ups for SDA and SDC, do I need to add additional pull-ups near to

this part  when routing I2C?  I'm considering adding this part to an existing design so I wanted to check to be safe.

Thanks,

- Andy

5 Replies

  • Hi Andy
    I am not sure i am clear on what you mean. BT11 is the battery and node 2 is connected to ground. The pfet allows the battery connect to the system and it appears redundant to me and not necessary except i am missing some thing.
    4.7 k pull-ups should be good with a 3.3V pulll up voltage.
    thanks
    Onyx
  • In reply to Onyx Ahiakwo:

    Hi Onyx,

    Thanks for the info.

    BT1 is the battery connector in the schematic with +ve (term: 1) and -ve terminal (term:2 ). I don't see the -ve terminal is routed or shorted to GND which I was expecting.

    - Andy

  • In reply to Andy Sarangi:

    Hi Andy,

    I am seeing BT2 connected t ground. Are we looking at the  same schematic?

    thanks

    Onyx

  • In reply to Onyx Ahiakwo:

    I don't see this connection (BT1: net2 to GND) in the Altium Layout. That was my question. There I see a pin something called "ALIGN" it is not connected to GND or to BT1: net2. Thanks Onyx for investigating it.
  • In reply to Andy Sarangi:

    Hi Andy,
    Pls go off what is in the schematic as that is what is correct and how the circuit should be connected.
    thanks
    Onyx

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.