Hi There!
I'm using the TPS92410 for a design working at 120VAC and I've found a problem in the over voltage protection section. It recommends to use Rground as 121K and then calculate the Rdrain using the equation. 121E3 * ((120-1.5)/1.5) = 9560000 (9M56) ] but in the suggested Figure 12. "Application schematic" the value is 2M!!
Is it wrong?
Kind regards,
Miguel