Part Number: IWR1443
Hi,
In mmWave Sensing estimator, When I increase the no of TX from 1 to 2 in the configuration, I see that the below changes,
1. The bandwidth increases by almost 2.3 times
2. The sampling frequency increases by almost 3 times.
3. The IF frequency also increases by 3 times.
I would like to know whether this increase is because it assumes the TX to be operating at the same time?? Otherwise, I see no reason for this increased values. The no of samples per chirp in these cases remain the same.
Since I am not planning to use the TX at the same time, and will be operating in time multiplexed format, I dont see the requirement to increase the bandwidth, sampling rate or IF frequency. The increase in frame time and radar cube size is acceptable.
If there any mistake in my assumption??
Thanks in Advance,
Santhana Raj