Hello,
Could you please let me know the min/max switching frequency at heavy load?
According to the datasheet figure 3~6 , is the fsw(min) about 1.1MHz and fsw(max) about 1.5MHz?
Best Regards,
Ryuji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ryuji,
it's a pleasure to support you. Figure 3 to 8 in the datasheet show the switching frequency dependency with the load current Iout and input voltage Vin and output voltage Vout. The combination of these 3 conditions establish the switching frequency regime. Furthermore also the passives influence the switching frequency, so keep in mind that the pictures refer to this configuration: L = 1 µH, Cout = 22 µF
Hence, you should identify the graph closer to your case's operating condition and refer to that one to estimate the switching frequency. Example:
Vout=1.8V ; Vin= 2.8V : Iout=1A to 3A -> figure 3 fits -> fmax=1.5MHz circa ; fmin=1.25 MHz circa
Enjoy your design!
Best Regards,
Emmanuel