This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLV713P-Q1: About "maximam output current limit"

Expert 1635 points

Replies: 1

Views: 235

Part Number: TLV713P-Q1

Hello Team,

How should the maximum value of the maximum output current limit be considered?
Only the minimum value is indicated in the datasheet.
The device is TLV71333.
Figure 16 in the data sheet is a typical value, isn't it?

Best regards,
Kato

  • Hi Junya,

    This device is rated to output a current at 150mA. The current limit is the maximum current it can source before the output current being limited. The reason datasheet only has the minimum 175mA spec is because the device is tested to be able to output 175mA. The device should be used at 150mA load max and datasheet allows some margins here.

    Figure 16 is only tested at 25C and you can consider it as typical values.

    Regards,
    Jason Song

    Please click the "Resolved" link at the bottom of this post if I have answered your question.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.