I have questions about inductor of TPS54A20.
In datasheet p.25, we use DFE252012F-R33M.
In datasheet of DFE252012F-R33M, Rated current(Isat) is 7600mA.
And Rated current (Itemp) is 5100mA.
But, in datasheet of TPS54A20 p.25, Saturation Current Rating is 8.5A.
Question 1.
Please tell us the reason of 8.5A.
Question 2.
Please tell us the definition of Saturation Current Rating in TPS54A20 datasheet p.25.
Question 3.
8.5 A indicates either Rated current(Isat) or Rated current (Itemp)?
Best regards,
Takahiro Nishizawa