Is the 1.5V of the ADM(limit) derived from or proportional to the 3V reference voltage?
Both are specified as +/- 5% tolerance
If derived then: If the 3V reference is at 3V +5%, then the 1.5V ADIM(limit) will be at 1.5V +5%
If separate and independent: Then 3V can be at 3V +5%, while the ADIM(limit) can be at 1.5V -5%
Can TI answer this?