This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG5200: Reference Design (TIDA-00913)

Part Number: LMG5200
Other Parts Discussed in Thread: TIDA-00913

Hello team,

my customer has rise the following questions below please advise back:

1.What input current of the LMG5200MOFT should receive?

a.Pin 4-Hi

b.Pin 5-LO

c.can I directly connect the Pins of the LMG5200MOFT to the TMS320F2837xD?

d.What is the reason that you connect the SN74AVC8T245RHLR between DRIVER (LMG5200MOFT) and MCU (TMS320F2837xD)?

 

thanks in advance and regards,

Shai 

 

  • Hi Shai,

    To answer you cursomer's questions:

    a&b) the LMG5200 HI and LI pins are logic high impedance pins, consider these ~2pF and min 100 kohm to ground, so the current really depends on the frequency but it will be very low.

    c) if the I/O voltage is kept above 3.14V as per spec your lowest output voltage out of the I/O pin is above 2.5V, this will be sufficient to trigger the logic threshold for the LMG5200 (2.22V max). Given this, it is possible to drive the LMG5200 directly.

    d) as I don't have much information about this project I assume  SN74AVC8T245RHLR is there as a buffer to break a long run between the micro and the power stage, also it might be there to increase the dynamic range and reduce pulse width distortion. This depends on what the Vdd power rails look like under all conditions.

    I hope this answers your question, but please feel free to reach out if you have more questions!

    Best regards,

    Alberto

  • Hello Alberto,

    Thank you for solve my issues, I was wondering if it possible to purchase the www.ti.com/.../TIDA-00913 It can definitely save me some
    time?
    waiting for your kind response, thanks in advance.

    BR
    Shai
  • Hi Shai,

    the TIDA-00913 is available as an orderable EVM under the part number:

    BOOSTXL-3PHGANINV

    Please let me know if you have any issues ordering this.

    Thank you and best regards,

    Alberto

  • Great, thanks for let me know.

    BR
    Shai