Other Parts Discussed in Thread: CSD18537NQ5A
Hi Support,
I designed the circuit of TPS40170QRGY IC dc to dc converter with the help of WEBENCH.
Our Requirement.
12V INPUT
3.3V OUTPUT
6A OUTPUT CURRENT
Here I attached the design we cant get the 3.3V output voltage. There is no shorting or no component damage.
Even I done below change and check the output but its not helpful to me.
- Give REG_2_ENABLE Externally.
- SS Pin Cap 2.2nf also check with 47nf.
- Check with R455 6K OR 5K.
- Put 0Ohm Resistance at R768 & R767 0Ohm.
Can you help me to verify the design and give some suggestion?
Here is the design