This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55010EVM-009: own current consumption

Part Number: TPS55010EVM-009
Other Parts Discussed in Thread: TPS55010

I have just tested the TPS55010 Evalboard. In idle-mode, only supply (5V) connected I measure input current 75 mA.

With 50mA load, I measure input current 128 mA @ Vin=5V. That do not comply with the high efficiency specified in the Evalboard documentation.

The eval board, is direct from the box, no modification. If measure with thermal camera, the heat is generated in the IC.