Other Parts Discussed in Thread: BQ78350, BQ76930, , BQ76200, ISO1540
Hello:
I have a 6s battery protection board is made of bq78350 and bq76930,when I reduce the voltage to 2.75 V/Cell, SMBUS communication is disconnected,but when I raise the voltage, the communication returns to normal. when the communication is disconnected, the VCC voltage of Bq76930 is normal 2.5V for bq78350.
So I wonder what caused this?