Part Number: TPS63020
Hi,
I am conducting the electrostatic test on products with TPS63020 installed.
I attach the material (excel sheet) of the circuit I created.
On the input side of the TPS63020, there is a charger circuit and a fuel gauge circuit.
Both the battery and the 5V fixed power supply are input to the TPS63020 input.
Attach the waveform (Excel sheet) of TPS63020 when performing the electrostatic test.
When static electricity is applied, the operation of the TPS63020 is latched.
Even if EN is switched, the state does not change.
However, when shutting down the power supply, it returns to normal operation.
I want to ask you a question.
What is the cause of latching the operation of the TPS63020 device when static electricity is applied?
Best Regards,