Other Parts Discussed in Thread: TPS61022, TPS61170
Hi,
We got a question from the customer about TPS61253A.
Could you help us?
[Question]
They are considering using TPS61253A under the following condition.
Vin=3.0V to 4.3V(1cell Li-ion) or 4.7V(ADP)
Vout=5.0V
Iout=30mA(typ),500mA(peak)
L=1.0uH
Mode=Forced PWM
- They need non pulse skip operation at this condition. How much is the minimum ON time of this device? They are thinking 4.7V input voltage is tough condition.
Best Regards,
tateo