Hi Expert,
Does the below data is right? Vin=2.3V, Vout=5V@1A
Pout=5W, Pin around=5/0.72=6.95W, the input current will over 3A, But TPS61252 current limit maximum is 1.5A only.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.