This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LP5910: LP5910

Expert 1070 points

Part Number: LP5910

Hi

For the part LP5910-1.0DRVR 

It is not clear in the datasheet what is the max. output capacitor 10uF or 4.7uF (I`m using only X7R ceramic capacitor),if I want to use higher capacitor from 10uF for example 47uF it is possible?

Thanks

  • For the LP5910 the maximum output cap I would recommend is 10uF. Using a larger output capacitor may cause stability issues.

    Best Regards,
    Mark
  • Expert 1070 points

    In reply to Mark Sellers:

    Hi

    Can you recommanded similar part which i can placed higher output capacitor such 47uF?

    Thanks

  • In reply to Hen:

    Hi Hen,

    The TPS747 should work well in your application.

    Best Regards,
    Mark

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.