Hi Sir,
As shown, the change in CL will affects the switching rise time and fall time. In the rise time is 41 ns when the CL reaches 5000 pF, For the 6.78 MHz frequency, the cycle / 2 is more than half, but in the specification CL does not make it clear where the capacitor?
1. Could you ask where CL is? Is the output load capacitor ?
2. If yes, by the marking red circle is the output capacitor of the Boost converter. Does it affect the integrity of the output voltage waveform or ripple. Does it affect the output of the front gate driver?
3. In addition, the output capacitor of the boost converter is generally above the uF level, according to LM5114 specification CL changes 1000pF ~ 10000pF are far less than the uF level
4.Is there any risetime / fulltime equation for CL?
Thank you
Kevin