This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200: Output voltage setting resistor

Part Number: TPS61200

Hi,

Q1.When Vout = 5 V, is the recommended resistance value below?
  R1 = 1.8 MΩ,R2 = 200 kΩ

Q2.Is it possible to use R2 of 100 kΩ or less and R 1 of 900 kΩ or less?
I would like to use a small resistance value,if possible.

Best regards,
Seishin