Other Parts Discussed in Thread: TPS61253
Hello,
I'd like to use this boost converter to provide a 5V supply from a Li-ion battery to a circuit that may also be powered by USB, but I can't tell from the the block diagram if there are any conditions under which applying a little over 5V to VOUT may result in reverse current flow through the device back to VIN damaging the battery.
I'm guessing that if the battery voltage drops enough that the device is no longer able to boost it to 5V that the UVLO will kick in and the battery will be protected. And it seems like unlike the TPS61253, the gate driver on the TPS61253A is connected to VOUT as well as VIN, so presumably that would still be pulling the PMOS gate high to turn it off even if the battery is disconnected, and the body diodes of the mosfet would prevent reverse current flow, but I'm not certain because the datasheet doesn't show how the gate driver functions.