Hello,
In my customer, there is the possibility that the CSP and the CSN voltage is under the 3V (for example, 2V) at the cold crank condition.
If there is the heavy load at the cold crank condition and there is input impedance due to the cable between battery to board.Thus the voltage drop is occured.
They already increase input capacitors but they have space limitation in the board.
Thus, they couldn't increase capacitor anymore.
VIN is biased from the output of LM5122-Q1. Thus, we can keep the voltage of VIN in the recommended operation range.
Then I have the following questions.
(1)
I think that if wthe CSN-CSP voltage is less than recommended operating conditions 3V, we couldn't guarantee the Vcs-th1 and Vcs-zcd specifications.
Are there any other concerns?
(2)
Could you please let me know the power supply of internal current sense amp?
Is it from Vcc or VIN?
Best Regards,
Ryuji