Other Parts Discussed in Thread: BQ76925, BQ77PL900, BQ76930, BQ77905
I have 6 Li-ion cells (unprotected 18650) in series, each using a bq29732 wired as per the ’10.2 Typical Application’ diagram in the datasheet.
On inserting the cells for the first time, each protection circuit has to be individually enabled (as per ‘Caution in section 9.4.1).
In use if the series of cells are operated until one of the cell protection chips trigger (OVP,UVP,OCC,OCD or SCP), automatic recovery is not possible via a charger as there is now in effect an open circuit in the series of cells. The only recovery is as per the ‘Caution in section 9.4.1’ across the individual tripped cell.
Is there a way to use the bq2973x in series connected cells where self-recovery is required ?