Hi
My Customer has question.
[Table 4. Matrix of Output Capacitor and Inductor Combinations] recommend 1uH, 1.5uH, 2.2uH.
Customer can only use 1 uH or 2.2 uH because of the availability of Inductor.
Is it OK to use 1uH or 2.2uH with the following spec?
I think that either way is OK, but please comment if there are any concerns.
■SPEC
VIN=3.0~3.6V
Vout=3.8V
Iout=0.5A
Cout=20uF
Regard
T Kishi