This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TL5001: How to use a TL5001 as inverting controller ?

Intellectual 320 points

Replies: 2

Views: 715

Part Number: TL5001

Hello,

I want to replace MAX635/MAX626 by a TL5001, as I have seen that this controller can be used as inverting controller. Is there anywhere schematic example to obtain -5V from a 5V input ?

If I remember, I have seen a long time ago this kind of application in a datasheet with a TL5001...

Best regards,

JB

  •  See the attached schematic markup for inverting output. Basically the IC should reference to the negative output rail.

  • In reply to Youhao Xi:

    Thanks a lot, I will try as soon as possible.

    Best regards,

    JB

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.