Other Parts Discussed in Thread: PMP20566
Dear Sir:
I found reference design PMP20566 for TPS54335. Does TPS54336A also can support 12V or 5V input and -5V(0.6~1A) out?
Best Regard
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sure, you can use the TPS54336 to generate the -5V.
The difference between them is the frequency, so change the value of the components when you want to use TPS54336 to generate -5V with PMP20566