Q1) Please verify the following calculation
This is the datasheet-section I am dealing with:
Intention is to calculate the maximum positive and negative threshold voltage for R1 = 30k and R2 = 10k.
VIN = 5V.
TPS389001, NEGATIVE THRESHOLD (VITN) = 1.15 V, POSITIVE THRESHOLD (VITP) = 1.157 V
From the equations, VITP(MON) = VITP × (1 + R1 ÷ R2 ) = 1.157 * (1+30/10) = 5.35 V
VITN(MON) = VITN × (1 + R1 ÷ R2 ) = 1.15 * (1+30/10) = 4.6 V
Q2) What is the potential at VMON ?
Q3) What will be the scenario if VMON connected to VIN ?
Please explain in the contest of following image,