One of my customers is looking for some confirmation on the following:
Regarding implementing the approach laid out in "Remote Sensing for Power Supplies" (slyt467), to account for IR losses in the power-distribution-network from the SMPS to the SoC load, can we confirm if this approach is supported with the TPS62160QDSGTQ1?
If yes:
- TPS62160QDSGTQ1 has both a FB and VOS pin. Which would go to the load?
- VOS is listed as voltage sense and connection for control loop circuitry
- Looking for confirmation if one or both of these would be tapped off at the load
Note- the remote sensor is located at approximately 1.5 - 2 inches from the load.