I'm designing in 2x LMZ14201H for +24<->+15 (and +24<->-15) rail conversions.
Equation 18 calculates the DCM & CCM boundary conditions... However the resulting values seem exceptionally high. My experiences with DCM in the past have it switch modes at low currents...
Here are my parameters:
Vin = 24V
Vo = 15V
Fsw = 300kHz (Ron=383kOhm)
Equation 18: IDCB = Vo*(Vin-Vo) / (2*15uH * fsw * Vin).
This yields IDCB = 625mA, on only a 1A Max supply!
This switcher operates in DCM up until ~62% of load current.
This seems quite high... Is there an error in the datasheet?