Team,
Do you have an excel calculator or something to estimate junction temperature for the TPS65320D-Q1? I am trying to see if i can run the DC/DC at 7.2V/650mA and the LDO at 5V/100mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
Do you have an excel calculator or something to estimate junction temperature for the TPS65320D-Q1? I am trying to see if i can run the DC/DC at 7.2V/650mA and the LDO at 5V/100mA.
Hi Julio,
I do not have a tool either. You can find a more detailed calcualtion in datasheet Section 8.2.1.2.11 Power Dissipation.
Please also consider that the LDO is supplied directly from VBAT in case the Buck is disabled, hence it needs to drop VBAT voltage to 5V (@100mA?).
Best regards,
Frank
Karl,Frank,
Appreciate the help, i was just wondering if there was a quick tool but ill go ahead and estimate with the provided equations. Thanks!