This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82740B: Current consumption issue

Part Number: TPS82740B
Other Parts Discussed in Thread: TPS63050, TPS3839

Hello,

I am having a consumption issue with the TPS82740B.

When the input voltage goes below 2.7V, the current consumption of the IC grows to aproximatly 240 uA.

Measurement conditions:

- The IC is configured to output 3V.

- IC enabled

- CTRL low (load output disabled)

Is this a known issue? 

Thanks in advance,

Alejandro