This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using UC3825DW IC for PWM generation at 350kHz for resonant full bridge inverter . This is operated at 17volts ac. Rc=1.39kOhms and Ct=1.22nF. This IC getting heating up very much. Results in frequency tarts at 362kHz-365kHz and reduces to 352 kHz over a period of operation in 5 to 10 minutes. This frequency variation is becoming a problem since overall unit operating time gets reduces due to input dc voltage variation. How to reduce this tolerance. I am unable to control the gain of the inverter.I have attached the my IC circuit diagram for your reference.
Hi John,
I am using SG3626 and gate driver transformer for driving the mosfets. Please suggest any other solution.
Regards,
Skanda