This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22675: About Line reguration question of LM22675.

Part Number: LM22675

Dear support member,

My customer use LM22675.

I have a question about line reguration.


Daimen is a 3 phase power supply,
The input voltage fluctuates at intervals of 8 ms at 0.1 V.
The output voltage fluctuated at intervals of 8 ms at 50 mV.

Is this normal behavior of IC?
If it is not normal operation,would you teach me the reason?

Specification condition
Vin: 27 V
Vout: 5 V
Iout: 1A


Best regard.
Bob Lee