Other Parts Discussed in Thread: TPS3700-Q1, TPS3702-Q1
Hi There,
I am using the LP5912-Q1 as a 1V2 linear supply off of a 1V8 PMIC SMPS output.
Looking at the PG function of the regulator I think I understand this as : the PG is low when the output voltage is below the PG(LTH) and goes high when above the PG(HTH) i.e at nominally 1V2, it will be HIGH .
If say due to an internal fault , the output climbs to 1V8 , will the PG remain high?
This is not typical of TI regulators, where normally the PG is only high (valid) if the output voltage is within say, 10% of the target value?
Can you explain this rational? Or have I misunderstood something here?
Also, is there more detailed information on the variation of the PG(HTH) or PG(LTH) and the tP(PGD). There are only typical values in the data sheet.
Many thanks in advance for your time and expertise.
Ross