This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B4250-Q1: do we have compatible part to S1212B?

Intellectual 1330 points

Replies: 1

Views: 388

Part Number: TPS7B4250-Q1

we try to find compatible TI part for 

S1212B

"www.ablicinc.com/.../S1212B_D_E.pdf"

ABLIC

S-1212B33-M5T1U

SOT-23-5

ABLIC

S-1212B50-M5T1U

SOT-23-5

there is TPS7B250-Q1 with similar input range, but the output current is not as much.

S-1212 max output current @ 250mA, is there non- Q1 part?

1 Reply

  • Hey John,

    Does this need to be pin-to-pin compatible? 

    If not, I'd suggest the TPS7B82-Q1 for supplying the 5V rail. We do plan on creating a 3.3V option as well.

    In general, the SOT23 is not a great package for dealing with power dissipation.

    Thanks, Aaron

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.