Part Number: FUSION_DIGITAL_POWER_DESIGNER
After reinstallation of FDPD ver.7.0.18 to ver. 7.0.25 we are facing several troubles (we use UCD90120A):
- it doesn`t plot correct values from OVW, OVF, OCW, OCF,... stored in "configure device", but it plots values from device/rail #1 for all rails
- ignoring stored values Max Y, Min Y
- writing value 6.72 ohm into current measurement doesn`t work, we read back always 10 ohm
Here is example (image_1.jpg) when FDPD monitor display for rail 102d/#5 (3.3V) (plot on the right side) limits for OVW, OVF,... from rail 101d/#1:
Here is the example when I change (rail 102d/#5) value OVF (from 1.00V to 4.00V) and click on write, then value OVF is changed also on the left (101d/#1) and I see OVF.
If I change on the left (rail 101d/#1) OVF back from 4.00V to 1.00V and I click on the write then the value on the right side is changed (rail 102d/#5) and OVF for rail 101d/#1 disappears:
In the window Configuration - Monitor is everything o.k.: